Soft Starter 3RW44 PCS 7 Library V8.0 +
SP1
Instructions on Installation and
Use
The
information and notes contained here are more up-to-date and therefore valid
compared with information in other documents.
Please read
the instructions carefully as they contain important information on installation
and use of the software.
Table of contents
1.2
New features and
alterations compared to previous versions 3
1.2.1
What is new in
Soft Starter 3RW44 PCS 7 Library V8.0 + SP1?. 3
1.3
Information on
the documentation. 5
1.4
Information on
the sample project 5
3.1
Additional
information on the software certificate. 8
5
Technical
Assistance Low Voltage. 9
The
information and notes contained here are more up-to-date and therefore valid
compared with information in the online help.
The
properties of the library Soft Starter 3RW44 PCS 7 Library V8.0 +
SP1 for SIMATIC PCS 7 V8.0 + SP1 &
Advanced Process Library V8.0 SP2 are in
essence:
·
Entire conformity to the PCS 7 driver
concept
·
Follows the motor blocks design of the PCS 7
APL Library
·
Faceplates based on the faceplate
designer
·
Supports all 3RW44 soft starter control
functions
The block
library contains control blocks (SSOprtn), a
measured-value block (SSMeas), a statistics block
(SSStat) with corresponding faceplates for the
integration of 3RW44 Soft Starters. The blocks support German and English. The
user documentation is available in German and English.
The
following are the blocks that support both PROFIBUS & PROFINET enabled 3RW44
soft starter devices.
Block Library
The library
contains following blocks:
|
Hardware |
Comment |
Name |
Number |
|
Soft
Starter |
3RW44 Soft Starter Diagnostics |
SSDiag |
FB1325 |
|
3RW44 Soft Starter Common Operation functions |
SSOprtn |
FB1326 | |
|
3RW44 Soft Starter Measurement |
SSMeas |
FB1327 | |
|
3RW44 Soft Starter Statistics |
SSStat |
FB1328 | |
|
3RW44 Soft Starter Channel block |
SSChn |
FB1329 |
These
blocks provide integration of Soft Starter function.
|
Soft Starter Function |
APL for Basic Integration |
Integration of Soft Starter function via Soft Starter 3RW44 PCS 7 Library V8.0 + SP1 Blocks |
|
Direct soft starter |
MotRevL |
SSDiag, SSOprtn, SSMeas, SSStat, SSChn |
Refer
to the User documentation for a function description or the online
help.
This
chapter gives brief information about the most important enhancements of Soft Starter 3RW44 PCS 7 Library V8.0 +
SP1 compared to previous
version.
New features
1.
Support of Soft Starter PROFINET device.
The
following functionalities are supported in SP1, for PROFINET
devices
·
New diagnostic messages related to FW update
and Energy saving functions has been added.
·
Log book data shall be read upon ReadData request instead of cyclic
update.
·
Logbook entries are displayed for each entry
along with Time stamp <HH:MM:SS>
·
Module drivers for PROFINET device are updated
in the objects and action lists for the driver wizard of
CFC.
2.
Read/Write record error status is displayed at
output parameters RdErrStat/ WrErrStat.
3.
Two reserve variables (ReserveIn and ReserveOut) have
been added in all of the function blocks for maintenance purpose to avoid the
interface changes in future releases.
Bug fixes
1.
The output parameters module fault SSDiag is reset correctly, when the device doesnt report
any more warnings or errors.
2.
Module driver files added to support
integration of 3RW44 when the DP mode of PROFIBUS is
S7_compatible.
3.
The Logbook data reading at SSStat is now acyclic. Reads data only on readdata request.
4.
The data reading of all datasets made acyclic
in all the function blocks (SSOprtn, SSMeas, SSStat and SSDiag).
5.
Slow speed Reverse command is disabled when
Group fault is active at device and Emergency start is not
active.
6.
Control diagnostic data, Device diagnostic
data, Parameter diagnostic data and Protection diagnostic data shall be updated
upon read data request.
7.
Text at faceplate shall be displayed in English
language when the WinCC configured language is other
than German.
8.
Missing named interconnections for SSChn, SSOprtn blocks at Template
have been added.
9.
The description of parameters at SSStat and SSMeas block has been
aligned according to the Soft Starter manual.
10.
Incoming/Outgoing event data is displayed at
Logbook view at SSStat.
11.
User authorization levels for Delete Trips
and Delete Events buttons changed to Level6.
12.
DiagDir parameter
name has been modified to DiagOprtn in SSDiag and SSOprtn
blocks.
13.
When the Soft starter device is in Local mode,
User has to Execute Read data command at SSOprtn
faceplate to monitor the status of commands executed at Local
mode.
14.
If Motor is running in Local mode and Process
image output is not updated at SSOprtn function block,
SSOprtn standard faceplate view displays the Motor On
status.
15.
Additional diagnostic messages have been added
related to Control, Parameter, Device and Protection
diagnostics.
Steps to be done for updating existing PCS 7
projects
|
No. |
Action |
Details |
|
1 |
Open the CFC chart |
|
|
2 |
Drag and drop the changed block (see the table below) from the CFC catalog in your project |
This triggers the update mechanism to update all instances of current block. |
|
3 |
Open OS
project editor at
WinCC explorer |
Closing this dialog by pushing OK-Button triggers update of faceplate files |
|
4 |
Open C editor at WinCC explorer (WinCC Explorer > Global Script > C-Editor) |
This re-generates headers for faceplate files |
|
5 |
Compile and download entire AS program |
Compiler: · Scope: Entire program · Generate module driver activated Download: · Download mode: Entire program |
|
6 |
AS Stop |
YES |
|
7 |
OS Compile |
YES Scope: · Entire OS · With memory reset |
List of changed
blocks
|
Number |
Name |
Block Version |
Interface change (AS stop
necessary) |
|
FB1325 |
SSDiag |
1.1 |
Yes |
|
FB1326 |
SSOprtn |
1.1 |
Yes |
|
FB1327 |
SSMeas |
1.1 |
Yes |
|
FB1328 |
SSStat |
1.1 |
Yes |
Problem description:
ModF_Act is set to '1' at SSDiag on warm restart of PLC when Soft Starter device is
connected using PROFINET CP.
![]()


Solution:
Please use
integrated DP/PN interfaces (PLC) for device
communication.
![]()

Information
about how to use blocks is given in the Programming and Operating Manual for
Soft Starter 3RW44 PCS 7 Library V8.0 +
SP1. They can be found in the internet.
Pleas follow this link: https://support.industry.siemens.com
and search for
Soft Starter PCS 7.
All
information about working with the blocks can be found in online help. You can
open online help in STEP 7 as context help for every block using F1 key or
question mark button. The complete help can be reached via button help
topics in the window of context help.
Once the
library is installed, a sample project Softstarter_Example is made available in the following
path
<drive>:\SIEMENS\Step7\Examples\
The project
has the necessary configuration details and all the interconnections of blocks
with its associated driver blocks. Hence the same can be used for reference.
The
project has instances of signalling, channel and driver blocks (SSOprtn, SSDiag, SSMeas, SSStat and SSChn).
The
3RW44 Soft Starter is inserted and configured along with its associated
components, GSD/EDD files and Object Manager files in the HWConfig.
The
library supports the functions of 3RW44 Soft Starters (PROFIBUS and PROFINET)
that are integrated using Object Manager files or using GSD files or EDD
files.
|
Configuring
the 3RW44 Soft Starter | ||
|
On
DP Master System (DP Interrupt mode as DPV0/DPV1)
using |
Behind
Y-Link (DP Interrupt-mode as DPV0/DPV1) using |
On
PROFINET I/O System* using |
|
·
Object
Manager file ·
GSD
files ·
EDD
files |
·
GSD
files ·
EDD
files |
·
Object
Manager file ·
GSD
files ·
EDD
files |
*
The operation behind the Y-Link is not possible in case of PROFINET.
|
Soft Starter PROFIBUS DP GSD files | |
|
SIEM80D?.GS? |
siem80d?.gs? |
|
SI0180D?.GS? |
si0180d?.gs? |
Download
link: https://support.industry.siemens.com/cs/#document/113630
Soft
Starter PROFINET IO GSD file: GSDML-V*-SIEMENS-3RW44PN*.XML
Soft
Starter EDD files (PROFIBUS and PROFINET):DP_PN_Switch_Siemens_DSStarter_V03.00.00.00
Download
link: https://support.industry.siemens.com/cs/#products?dtp=Download&pnid=16214
GSD, GSDML
& EDD files for 3RW44 Soft Starter can be found in the internet. Please
follow this link: http://support.industry.siemens.com
and search for
·
Soft Starter GSD or
·
Soft Starter GSDML or
·
Soft Starter EDD
The
following PROFIBUS DP/ PROFINET IO communication modules with firmware versions
specified below are used for communication with the 3RW44 Soft
Starter.
|
Firmware
version |
DP Interrupt
Mode |
Configuration |
|
*E03*:
Firmware µC1
- BS01-3RW44-Z100 µC2
- BS01-3RW44-Z03 µC3
- BS00-3RW44-Z00 *E04*:
Firmware µC1
- BS01-3RW44-Z100 µC2
- BS01-3RW44-Z04 µC3 - BS00-3RW44-Z00 |
DPV0/DPV1 (PROFIBUS) |
On Master System |
|
*E04*:
Firmware µC1
- BS01-3RW44-Z100 µC2
- BS01-3RW44-Z04 µC3 - BS00-3RW44-Z00 |
DPV0/DPV1 (PROFIBUS) |
Behind Y-Link |
|
*E01*:Firmware µC1 -
BS01-3RW44-Z110 µC2 -
BS01-3RW44-Z01 µC3 - BS00-3RW44-Z00 |
PROFINET |
On PROFINET IO System |
The library
supports the following 3RW44 Soft Starter device article
numbers
|
Article
number |
|
3RW4422-*BC** |
|
3RW4423-*BC** |
|
3RW4424-*BC** |
|
3RW4425-*BC** |
|
3RW4426-*BC** |
|
3RW4427-*BC** |
|
3RW4434-*BC** |
|
3RW4435-*BC** |
|
3RW4436-*BC** |
|
3RW4443-*BC** |
|
3RW4444-*BC** |
|
3RW4445-*BC** |
|
3RW4446-*BC** |
|
3RW4447-*BC** |
|
3RW4453-*BC** |
|
3RW4454-*BC** |
|
3RW4455-*BC** |
|
3RW4456-*BC** |
|
3RW4457-*BC** |
|
3RW4458-*BC** |
|
3RW4465-*BC** |
|
3RW4466-*BC** |
This
version is provided in two languages and runs under any PCS 7 Version listed in
4.2.
|
Package |
Article
Number |
Scope |
|
Engineering
Version |
3ZS1 633-1XX02-0YA0 |
1 Setup CD 1 Certificate of License 1 Web download |
The
software certificate is part of the contract for use of software products
against a single payment which contract is part of the scope of delivery. It
states licensed software components with their warranty
classes.
The
customer is not authorised to make any changes to the
software.
The
software product key number must be quoted in
correspondence.
For the
Open Source agreement please refer to the
Readme_OSS.doc in PCS 7 and Soft Starter 3RW44 PCS 7 Library V8.0 +
SP1.
There is
Engineering and a Runtime License in form of a Certificate of License
available as Single License for Soft Starter 3RW44 PCS 7 Library V8.0 +
SP1.
Engineering License
A Single
Engineering License allows the installation and usage of the library on an
Engineering Station (ES).
Runtime License
The Runtime
License is delivered together with the Engineering Software. One Single Runtime
License allows to run the AS blocks in a PCS 7 automation system and to use the
OS components (block symbols and faceplates) on several Operator Stations
(OS).
Further
Runtime Licenses are required to run the AS blocks on further PCS 7 automation
systems (AS). Please refer to the table below for the article numbers of further
licenses:
|
Article
number |
Description |
|
Engineering
Software (3ZS1
633-1XX02-0YA0) |
Soft
Starter 3RW44 PCS 7 Library V8.0 + SP1(ES)
|
|
Runtime
Version (3ZS1
633-2XX02-0YB0) |
Soft
Starter 3RW44 PCS 7 Library V8.0 + SP1(RT)
|
The
hardware requirements of SIMATIC PCS 7 apply for the
installation.
The use of
the software Soft Starter 3RW44 PCS 7 Library V8.0 +
SP1 requires as a minimum SIMATIC PCS 7 V8.0 + SP1 &
Advanced Process Library V8.0 SP2.
The
SOFTSTARTER ES Premium software is necessary to be able to integrate 3RW44 as an
S7 slave using an object manager (OM).
This
library is incompatible with
·
3RW44
Soft Starter PCS 7 Library V8 Migration V8.0
·
3RW44
Soft Starter PCS 7 Library V8 Migration V8.0 + SP1
·
and
lower versions
Please
uninstall the incompatible library first, before installation of Soft
Starter 3RW44 PCS 7 Library V8.0 + SP1.
Parallel
use of an incompatible library is not supported and leads to a fail in module
driver generation.
Siemens AG
Technical Assistance
Phone: +49 (911)
895-5900
Fax:
+49 (911) 895-5907
E-mail: technical-assistance@siemens.com
www.siemens.com/industrial-controls/technical-assistance